1/4/2018 9:24 AM | |
Posts: 664 Rating:
|
Dear PISCEAN 2010, Thanks for your valuable reply.. I have checked the parameter list, 318.0[Showing in expert list instead of 318.8] Dynamic Following error monitoring tolerance : 2mm Positioning set point send through Profibus. Its the running machine. No alarm/fault displayed in PLC/Drive. Machine axis is traversing. I am attaching drive backup. Thanks&Regards, AttachmentA.txt (276 Downloads) |
1/4/2018 9:34 AM | |
Posts: 664 Rating:
|
Please let me know how the synchronization done, and how can i identify to which drive its synchronizing? Its describing about coupling option, what is the meaning and working of coupling. I am not that much worked in Simodrive, so please guide, how they have set the set point over the communication [Profibus Data] and what profibus frame size have set. And in block they have defined Traversing block with some positioning value, how can i identify, where it started in drive side?. Thanks&Regards, AttachmentB.txt (270 Downloads) |
1/5/2018 5:28 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello List, From the drive parameter back up files, I understood the working of system is as follows. 1. A drive axis positioning synchronisation with master is activated via profibus bit PosStw.4 2. B drive absolute positioning with master is activated via profibus but PosStw.4 Position control word is transfered to both the drives via profibus. In your case, Step 7 PLC acts as a master. Since the axes has lost positioning synchronisation, refer positioning status bit i.e. PosZsw.3, you are not able to move axis. Please check/study PLC logic as how the set point is calculated & control signals are transfered to drive, which sets the synchronisation. HTH. Hello, Dynamic following error = It is the comparison between measured & calculated position value. When the difference exceeds the value set in P0318 : 8, the output signal in positioning status words becomes low. So please check the encoder of your drive. |
Last edited by: PISCEAN 2010 at: 1/5/2018 7:47:53 AMLast edited by: PISCEAN 2010 at: 1/5/2018 9:09:13 AM |
|
Follow us on