6/4/2008 7:48 AM | |
Posts: 55 Rating:
|
Yes, very much possible to take image backup by Norton Ghost software or some other sw. of course, m/c screen and all other file are preloaded in MMC103 , hence after removing - m/c can't be run. |
6/4/2008 8:17 AM | |
Joined: 12/5/2006 Last visit: 5/26/2023 Posts: 177 Rating:
|
Thank you Sir, But my Question is why the Battery is Used , and If I Connect My PC with MMC startup Software the User Screen ( Machine Screen) Not Coming. It Has Stored Were. How to Take Backup. Regards Dharma |
6/5/2008 10:42 AM | |
Joined: 1/19/2008 Last visit: 9/15/2025 Posts: 998 Rating:
|
HI, It depends how the user screen was programmed as to where it will be stored but it will always be stored on the hard disk as part of the MMC. If you run a different mmc copy like on your pc the screen does not exist on your pc and so cannot be loaded. If you take a full mmc disk copy it will also copy the user screen. Is the battery you talk about just the clock backup battery or is it something else ? |
6/6/2008 2:00 PM | |
Posts: 63 Rating:
|
Dear Dharma, 1. It is possible to take hardisk backup . You should have ghost 8.3 aonnecte it via usb run it on pc take image. However some time there is chance of system file missing. So you may need win95 strtup disk and from that you have to transfer sys file. 2.User screens are dependent on machine builder. So it required to check on which platform oem developed same. it may be with easymask, visual basic or hmi extended. and based on this suggestion can be gven. rgds vki |
6/7/2008 4:25 AM | |
Joined: 12/5/2006 Last visit: 5/26/2023 Posts: 177 Rating:
|
Hai Viki Thank you . IfI Remove the Hard Disk from system and Make an Ghost back up using XP. the User Screen what will Happen . it will lost or it will remain in Hard Disk. Because I had mentioned in my Lat Post That is It has Battery. Regards Dharma |
8/16/2008 3:59 PM | |
Posts: 63 Rating:
|
Dear Dharma, |
Follow us on