9/13/2018 5:48 PM | |
Posts: 4 Rating:
|
I have a the same issue but have not been able to get it resolved. I am trying to use all four PTOs on the signal board. I have a 1214 DC/DC/DC CPU with the DQ4 Signal Board mounted to it. I can add the "Technology Objects" but when ever I try to enable them they fault with configuration errors. I DO have two PTOs working controlling two stepper drives. I copied the existing ones and let the software correct the addressing. I have 2 working really need to get the other 2 working. ------------------------------------------------------------------------------------------ AttachmentScreenshots.zip (439 Downloads) |
Last edited by: Jen_Moderator at: 9/14/2018 7:48:34 AMNew subject after splitting Last edited by: Jen_Moderator at: 9/14/2018 8:05:37 AMRemoved all attachments and added them as a sample here. Last edited by: Jen_Moderator at: 9/14/2018 8:22:42 AMEdited headline |
|
9/13/2018 7:40 PM | |
Posts: 4 Rating:
|
How do I change DB numbers. I have looked all over. The motion object was copied x3. The DB numbers corrected. The PTO references corrected. |
9/13/2018 8:05 PM | |
Posts: 4 Rating:
|
I did find where to manually change the db numbers That was not it. |
Last edited by: Dgoodrow at: 9/13/2018 8:10:08 PM |
|
9/14/2018 1:04 PM | |
Posts: 4 Rating:
|
The PLC was reset and the hardware downloaded, Everything good now. Thanks for the help. |
This contribution was helpful to
1 thankful Users |
Follow us on