5/7/2019 11:26 AM | |
Joined: 6/17/2014 Last visit: 10/27/2021 Posts: 77 Rating:
|
Hi, Ok thanks. Best regards |
5/9/2019 2:47 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, there is another thing you can check. I hope I can explain it detailled enough. I attached two pictures in the zip folder (L+ and M). Please take a voltmeter an check the voltage when your problem mPCIe card is plugged and the IOT is connected to your powersuplly. The ground pin to measure is the one squared in the picture M+. The measured voltage should be 3.3 V. If it is lower than the mPICe card needs too much of the interal provided one and the IOT2000 cannot be powered on. If it is 3.3V we have to loop back and search for some other reasons. Best regards! AttachmentIOT.zip (259 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on