4/28/2020 1:31 PM | |
Posts: 1 Rating:
|
Hello all, is there someone who can help me? I'm new from this platform!! I've a sketch that run well on arduino and web server but the same on iot2020 has problems. CLIENT MODE: from php file via ajax I've to send command to relay (arduino relay filed connected to iot2020), the problem is that the commad run well I'able to open my garage door with relay, but the response from iot to php page always return ERROR with "net::ERR_CONNECTION_RESET 200 " on chrome console. whats wrong? SERVER MODE: i'm not able to connect: always error connection via serial monitor!! In this case I've to read an rfid ID tag and send the info to the remote web server via https/http but nothing, always not connected. For well doc please referred to the attached files. (sketch, html file) Thank a lot in advance!! Iacopo AttachmentIOT2020.zip (287 Downloads) |
Follow us on