7/28/2020 9:27 AM | |
Posts: 10 Rating:
|
I've attached it in a txt file. Since then I've found this guide: https://www.plcnext-community.net/index.php?option=com_content&view=article&id=283:how-to-use-your-own-security-certificate-with-an-opc-ua-server&catid=78&Itemid=366&lang=en with which I can generate certificates, but these, similar to the keys that are on my laptop, only have coded material, key first then certificate, while the IOT's certificates contain plain text data too, and contain the key in a different code.
vs.
When replacing a couple of the IOT's certificates in the node folders with this, I get a "BadDecodingError" error instead of the above pictured certificate. It may also be of note that when first adding the server in UAExpert, I get a "Replaced Hostname" alarm: "The hostname of the discovery URL used to cal GetEndpoints (iot2000) was replaced by the hostname used to call FindServers (192.168.200.1). Do you also want to replace the hostnames of the EndpointURLs with this hostname?", and I can only access the server if I click yes here. Not sure if this could be another point where the HMI straight up refuses the connection. Attachmentbackup.txt (255 Downloads) |
Last edited by: Holko at: 07/28/2020 09:31:28 |
|
Follow us on