12/18/2020 4:47 PM | |
Posts: 18 Rating:
|
I want to mount a 1TB USB to port X60 USB on the IOT2040 and store data to an SQLite3 database there. I followed this walkthrough and when I ran "ls /dev | grep sd" it showed both /dev/sda and /dev/sda1. I then made a directory called iot2040 and tried to use "mount /dev/sda /iot2040. I received this error... mount: /iot2040: wrong fs type, bad option, bad superblock on /dev/sda, missing codepage or helper program, or other error. From my searches online it sounded like I needed to create a file system so I ran "mkfs.ext4 /dev/sda" and got this.... mke2fs 1.44.3 (10-July-2018) 64-bit filesystem support is not enabled.The larger fields afforded by this feature enable full-strength checksumming.Pass -O 64bit to rectify. Creating filesystem with 256000000 4k blocks and 64004096 inodes Filesystem UUID: d195beb6-489a-42bd-926c-9df1df7f7659 Superblock backups stored on blocks: 32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208, 4096000, 7962624, 11239424, 20480000, 23887872, 71663616, 78675968, 102400000, 214990848 Allocating group tables: done Writing inode tables: done Creating journal (262144 blocks): done Writing superblocks and filesystem accounting information: I am now stuck on the following waiting for done. Is there a simple way to mount a USB to the IOT2040 that I am missing? Is there a simple way to do anything with the IOT2040? What am I doing wrong here?
|
Follow us on