1/15/2021 2:55 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Perhaps this thread might help: https://support.industry.siemens.com/tf//de/en/posts/et200s-faults/65306/?page=0&pageSize=10 Check the configuration and the available hardware. Is the end resistor used? Best regards, Wizard |
1/17/2021 5:53 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
The machine was previously working then started to have this error bit by bit now my client can't turn on the machine, maybe after trying for a while the error will disappear for a bit but then it comes back so I don't think is an error in configuration I think it's more on a module that isn't working correctly but I just don't understand that manual with the code that I'm getting |
Follow us on