1/19/2021 10:13 AM | |
Posts: 7 Rating:
|
Hi, When loading the attached GSD in TIA Portal V16 "Device Configuration" a user is not able to edit some device-specific parameters such us Address in slave mode, ScenX: Address of Xst bit or register ScenX: Qty of bits or registers (Where X is a number between 1..20) Unless the user saves the program and restarts TIA Portal V16. This has happened to many GSD files I've tried to load previously AttachmentAGIL0834.zip (415 Downloads) |
Follow us on