7/2/2018 2:27 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating:
|
my cmr-2020 connected to a LOGO! BM I have tired several times to send a command for switching network inputs based on their VMs in the LOGO but every time it answered "No success" maybe its because of old-dated firmware? my firmware is 1.1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/2/2018 3:03:47 PMNew subject after splitting Last edited by: Jen_Moderator at: 7/4/2018 8:02:43 AM |
|
7/2/2018 2:46 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
The data format BIT (Bool) in SMS instructions is only available as of firmware version V2.0. Here you can download the latest firmware version (V2.1.5) for free: Firmware update V2.1.5 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) |
7/2/2018 3:22 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating:
|
The connection between LOGO and CMR is Ok because the commend for STATUS=RUN/STOP works. I have tired all of this form of commands: [Password=A] Command: A;LOGO=VM1,1,BYTE Reply: LOGO=VM1,1,BYTE: No Success Command: A;LOGO=VM1,1,BIT Reply: LOGO=VM1,1,BIT: Invalid Prameter Command: A;LOGO=VM1,1,WORD Reply: LOGO=VM1,1,WORD: No Success [the logo diagram attached] AttachmentCMS-LOGO_lsc.zip (370 Downloads) |
7/2/2018 4:11 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35940 Rating:
|
The correct syntax by using the datatype BIT is:
Do you have everything set up in the WBM for receiving SMS (see attachment)? Are the LOGO! and the CMR in the same IP address segment? AttachmentLOGO! 8 - Industrial Ethernet LOGO! CMR2020 _ LOGO! CMR2040_edition_2015_05_page86.pdf (433 Downloads) |
7/2/2018 6:52 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating:
|
Doesn't work! Command : Password;LOGO=VM6,1,BYTE Reply: LOGO=VM6,1,BYTE: No Success [the logo diagram attached] |
7/2/2018 10:33 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating:
|
Are there anybody? |
7/4/2018 2:14 PM | |
Posts: 30 Rating:
|
Have you "programmed" the outputs in cmr-2020, on the webpage? Because run/stop is a standard syntax but for write outputs you need to specify it on the cmr webpage Follow this and it should work https://cache.industry.siemens.com/dl/files/237/105074237/att_831074/v2/105074237_LOGO_CMR_en.pdf Attachment105074237_LOGO_CMR_en.pdf (343 Downloads) |
Last edited by: Pattedog at: 7/4/2018 2:17:27 PMLast edited by: Jen_Moderator at: 7/4/2018 2:46:42 PMAdded file as an attachment. |
|
This contribution was helpful to
1 thankful Users |
Follow us on