5/4/2015 8:09 AM | |
Posts: 29 Rating:
|
image 2 |
5/4/2015 8:30 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Please have a look at the following link: Which panels can communicate with a SIMATIC S7-1200 or S7-1500 in the TIA Portal? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
5/4/2015 12:46 PM | |
Posts: 29 Rating:
|
i cant able to find "connection mechanism"option under the "protection" menu Is GET/PUT function is the only option to communicate this type PLC ??. |
5/4/2015 2:16 PM | |
Posts: 29 Rating:
|
version of my HMI is v 11.0.1.0. and also i tried by upgrading it to 12.0. Do i need to upgade the firmware of CPU ?? |
5/4/2015 3:19 PM | |
Posts: 29 Rating:
|
Plz take a look at this. connection for that tag is not availabe, this is my problem. |
Follow us on