8/14/2014 7:42 AM | |
Posts: 7 Rating:
|
In our factory have an machine based work s5 95u and op17 panel. S5 95u don t have optional eeprom module After an long period without use (2 years) the backup battery its complet dead and i loss the program. I talk with the machine manufacturer and now have the original program.(can find in the atach) I transfer the program in follow order DB,FB,PB AND OB. The machine work now but after power off and again power on on op17 display have error system and the machine don t start. what can be the solution? Thank you very much AttachmentPBV.ZIP (556 Downloads) |
8/14/2014 8:17 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, which error message on OP17? Is the PLC in RUN or STOP? Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
8/20/2014 1:59 PM | |
Joined: 10/24/2011 Last visit: 12/16/2024 Posts: 71 Rating:
|
Hello Mario, some news ?problem solved? Jenda
|
Follow us on