6/11/2024 12:14 PM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi, as from TIA V19 it is possible to do indirect addressing of other ways. See the post Simple Sample and TIPs - WinCC Unified - DB Name Multiplexing |
Denilson Pegaia |
|
6/11/2024 12:15 PM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi, as V19 up2 it is also possible to debug Scripts in Visual Studio. The Visual studio extension (and the installation manual) are available at SIMATIC WinCC Unified RT Debugger TIP:
|
Denilson Pegaia |
|
1/12/2025 6:55 PM | |
Joined: 1/21/2013 Last visit: 9/6/2025 Posts: 4090 Rating:
|
Hi brzAA,
With the exception of some device-specific functions such as StartProgram, CreateScreenshot or File-Access, the scripts for WinCC Unified Comfort Panel can be used for WinCC Unified PC Runtime as well as for WinCC Unified Basic Panel. Kind regards |
This contribution was helpful to
2 thankful Users |
Follow us on