5/15/2021 2:09 PM | |
Joined: 6/2/2020 Last visit: 9/16/2025 Posts: 228 Rating:
|
Hello , I just want to know, I have a pressure switch which can provide 4-20mA. Now I just want to connect in AI card(6es7331-7KF02-0AB0) and this card is configured in all Channel-D. So how to do the connection so that I can get values from it? Should I connect 4-2mA on terminal 2 in AI Card. Any ground connect on terminal 3 in AI card. ------------------------------------------------------------------------------------------ |
Last edited by: Harry55 at: 05/15/2021 14:10:55Last edited by: Jen_Moderator at: 05/17/2021 10:30:19New subject after splitting |
|
5/17/2021 10:31 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Analog Card 6Es7331-7KF02-0AB0 connection is published within the conference SIMATIC S7-300 / S7-300F. Jen_Moderator |
This contribution was helpful to
1 thankful Users |
Follow us on