5/7/2021 12:14 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Sorry, not possible. The cpu can only be replaced (without changing hardware )by it's direct successor.6ES7314-6CF02-0AB0 Regards, Marcjan |
Problem solved? |
|
5/7/2021 12:21 PM | |
Joined: 10/22/2011 Last visit: 8/28/2025 Posts: 308 Rating:
|
Dear marcjan, Thanks for reply 6CF02 is also obsolete and successor is 6CH04, please check attachment waiting |
5/7/2021 10:12 PM | |
Joined: 3/28/2015 Last visit: 9/14/2025 Posts: 725 Rating:
|
Hello,
Yes,this is possible. |
Eng.Mohamed Ibrahim |
|
5/9/2021 4:48 PM | |
Joined: 3/28/2015 Last visit: 9/14/2025 Posts: 725 Rating:
|
Hello Marcjan, I did this work in our Labelling machine and succeeded. ------------------------------------------------------------------------------------------------------ Please have a look at the attached photo. 6ES7313-5BE00-0AB0 " The CPU type in the HW Configuration" Successor product 6ES7313-5BE01-0AB0 Successor product 6ES7313-5BF03-0AB0 Successor product 6ES7313-5BG04-0AB0 " The existing CPU type in the actual rack" The Procedures: 1-Turn off the Power. 2-Remove the old CPU S7 313-5BE00-0AB0 3-Install the new CPU S7 313-5BG04-0AB0 4-Insert MMC in the new CPU 5-Turn on the Power. 6-Execute the Memory reset. The machine will be run without any problems. ------------------------------------------------------------------------------------------------------- |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
4 thankful Users |
5/25/2021 7:56 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello Marcjan. It is possible in case the new CPU is a spare part compatible with the old CPU. It's not a rule to have a direct successor CPU to replace the old one without changing the HW configuration. All you have to know if the new part number is spare part compatible with the old one or not. Please check this link: |
Ayman Elotaify |
|
This contribution was helpful to
2 thankful Users |
Follow us on