3/4/2009 5:00 PM | |
Posts: 17 Rating:
|
Plase help how to use SFB3 TP IEC_TP in FB and the call into FC |
This contribution was helpful to
1 thankful Users |
3/4/2009 10:01 PM | |
Posts: 2661 Rating:
|
Hi salman92, You need to drag-and-drop SFB3:TP onto your ladder (FC, FB or OB)as shown in attached screenshot. An instance DB is needed for each call and I am not sure it'll work in a pure S7 scenario (without CFC). The preset time (PT) and elapsed time (ET) are double words in milliseconds. It is better to use the built-in timers in LAD/STL/FBD. Regards AttachmentIEC_TP_LAD.pdf (1245 Downloads) |
Follow us on