9/5/2009 10:50 AM | |
Posts: 5 Rating:
|
Dear all, I need to connect the analog output of an Allen Bradley Micrologix 1200 (from module 1762-OF4,see attachment) and need to connect it to an analog input of a 6ES7-331-7KF01-0AB0 module. It's a 4...20mA signal and it hasto go over multicable from the output card to input card(so not the same 24VDC supply for both plc's). Do I need to chose for 2 Wire transducer when setting up the analog input card, or 4-wire? Are there any other things where I have to pay attention for? thanks in advance, regards Attachment1762-OF4.pdf (507 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on