10/10/2014 3:09 PM | |
Joined: 9/22/2010 Last visit: 2/10/2025 Posts: 225 Rating:
|
Hello Jens, you need the license "Modbus/TCP PN CPU" with the order number 2XV9450-1MB02. The product is released for STEP 7 V5.5 or TIA Portal V13 Update 3 or higher. It is not possible to install the product for TIA Portal V11, but it is possible to migrate a STEP 7 V5.5 project containing the Modbus/TCP blocks to TIA V11. The following FAQ describes how to migrate such a project: How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the S7-300 and S7-400 CPUs and IM151-8 PN/DP CPU in STEP 7 Professional (TIA Portal)? You can find more informationabout the product and a demo versionhere: Modbus/TCP Regards, Sakura |
10/10/2014 3:17 PM | |
Joined: 1/5/2011 Last visit: 3/13/2025 Posts: 815 Rating:
|
Thanks a lot Sakura, is it also possible to copy them from the sample project? I find migratinga bitcumbersome... thanks in advance Kind regards, Jens |
Keep it simple and on-topic. |
|
Follow us on