4/30/2023 2:22 PM | |
Joined: 2/8/2009 Last visit: 1/10/2025 Posts: 9 Rating:
|
Good morning everybody. I have a similar problem, I'm trying to change the address of a 4DI card so that it starts from I0.4 to 0.7, and I get the same error message. If possible, what is the way? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2023 11:21:11New subject after splitting |
|
5/1/2023 1:53 AM | |
Joined: 2/8/2009 Last visit: 1/10/2025 Posts: 9 Rating:
|
The solution is... Configuring Hardware and Communication Connections STEP 7 (pg. 69) General Procedure: "Packing" Address Spaces Together 1. Select one contiguous range of modules whose addresses are to be packed. 2. In the Details view of the configuration table, click on the Pack Addresses button. The address areas for inputs, outputs, and motor starters are packed separately. - The beginning of the address area is defined by the address of each module that is selected first and has the form X.0. - If the bit address is not 0, the next (available) byte address from which the selected area can be inserted is used automatically, for example, (X+1).0. - If there is no other contiguous range, packing takes place automatically into available address spaces |
Last edited by: Chicão at: 05/01/2023 01:55:00 |
|
Follow us on