10/23/2024 9:42 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi AutoGen_2242618, In this case, I would recommend you to review the following FAQ that I share with you: I recommend you to review the information in the above link to see if it can help you. Best regards! |
If this Information really helps, you could use the Rate function |
|
10/23/2024 9:44 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Are you sure it is programmed with a TIA Portal version? Perhaps Step 7 v5.x Simatic Manager is used? (Edit: itafusna was quicker Best regards, Wizard
|
Last edited by: Wizard at: 10/23/2024 09:47:24 |
|
This contribution was helpful to
1 thankful Users |
10/23/2024 11:16 AM | |
Joined: 10/9/2024 Last visit: 4/6/2025 Posts: 9 Rating:
|
Yes. I went through that. but there also no option to know the version of CPU, that connected through CP 343-1 lean. |
Follow us on