3/17/2025 2:10 PM | |
Joined: 1/9/2025 Last visit: 3/20/2025 Posts: 4 Rating:
|
The simatic SD import of the new ladder s7dcl from version V20 does not import correct. If you export working (compiled) software (a function block with in it a couple of networks calling function blocks with the instance data stored in statics of the calling function block) and import the same file(s) it corrupts the software. It assumes you are referencing an instance datablock, instead of the static. (All by using a small openness api c# program, since it is not yet available in the version control interface). I tried the latest V20 update 1, but unfortunately this did not resolve the issue. The simatic SD makes generating ladder software a lot easier, but at the moment it is useless for this situation.
___________ split from Openness V20 Bug? |
Last edited by: AutoGen_7691503 at: 03/17/2025 14:13:12Last edited by: AutoGen_7691503 at: 03/17/2025 14:21:23Last edited by: Moderator_Lan at: 03/17/2025 14:56:12New question split into seperate topic Last edited by: AutoGen_7691503 at: 03/17/2025 16:26:42Last edited by: AutoGen_7691503 at: 03/17/2025 16:47:21Last edited by: AutoGen_7691503 at: 03/17/2025 16:48:14 |
|
Follow us on