3/24/2025 4:20 PM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
SIMATIC S7-1200 G2 Migration ToolThe Migration Package provides assistance for a complete modernization of a TIA Portal project from a SIMATIC S7-1200 to a SIMATIC S7-1200 G2. The Migration Tool is a TIA Portal Add-In consisting of a Migration Checker and an application that automatically implements the migration. When the Add-In is executed, existing program components are automatically transferred to a configured S7-1200 G2 for the user. However, manual adaptation of some program blocks is necessary. The “Migration Guideline” document provides step-by-step instructions for implementing the manual tasks. The explanatory video summarizes all the important points of the Migration Tool Add-In and the limitations it contains. In addition, the video provides assistance with the implementation, execution and interpretation of the results of the Migration Checker and Tool. |
This contribution was helpful to
2 thankful Users |
Follow us on