4/29/2018 8:33 AM | |
Posts: 2 Rating:
|
hii experts, i am developing a shutter opening and closing system by using plc s7 200. my i am usnig a NEMA 34 stepper motor to control the shaft which is connected with the shutter my project requirement is as follows 1.when Start switch is pressed the system should be ready for the task 2. then i want a selector switch for the direction control of the motor.(i.e. forward or reverse ) 3. if forward direction is selected then whenever a rotate switch is pressed the motor should rotate in forward direction as long as the rotate switch is pressed when we release the rotate switch the motor should stop ratating 4. similar operation for reverse direction. please can anyone help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/29/2018 4:11:04 PMNew subject after splitting |
|
Follow us on