11/7/2008 2:33 PM | |
Posts: 20 Rating:
|
Hi Mr. Pee.. as i see, this modification was not doing at "field" due i get a original copy of a listing from the machine original docs, and it are clearly marked. You mention LIR and TIR, so i can suposse, the code for this pb, may be allocated in a DB epromed and a startup time tranfer to the RAM space. Well i suspect, but as i kwon the first block executed after a reset, is OB1, if OB1 calling the DBs in Ram, a exepction is produced due the PB not ara allocated, so may be a sort of error trapping and calling a routine to load this PBs in RAM so at next restart is present? i think on OB20 as example. but OB 20,21 and 22 have: ; JU FB 19 NAME: WIED.ANL BE is a call to warm restart. but in OB2 /no called by any segment/ have a secuence of tranfers with L and T. i attach the code. OB2 is a special block? how are manipulated.¿? i not found any info abouth this block number. this PB can be transfer by: *The PLC2 to the PLC ram? *Setting via Parameters loaded in the CNC? Thank you by you expertise! Juanjo Attachmentob2.pdf (351 Downloads) |
11/8/2008 10:13 AM | |
Posts: 672 Rating:
|
Hi juanjoR I have some english manuals on pdf if it would help. |
11/8/2008 11:55 AM | |
Posts: 20 Rating:
|
hello Mr. Pee. thanks you very much for your offer abouth the manuals i accept it, i sent you a email. thanks again. Juanjo |
Follow us on