11/19/2019 7:51 AM | |
Posts: 1 Rating:
|
Distributed I/Os: End of the synchronization with a DP master/IO controller ERROR IS SHOWN WHEN DIAGNOSTICS OF THE CPU CURRENT STATUS OF THE CPU3152 PN/DP SF LED ON AND BF1 LED BLINKING TRYING PROFIBUS COMMUNICATION BETWEEN 315 2 PN/DP CPU AND IM-151 DISTRIBUTED I/O MODULE. PLEASE HELP ME.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/19/2019 08:09:16New subject after splitting |
|
11/19/2019 9:04 AM | |
Joined: 9/9/2014 Last visit: 2/12/2025 Posts: 246 Rating:
|
Hello) To get started, explore similar topics (there are answers to your question) Distributed I/Os: end of the synchronization with a DP master Profibus DP error End of synchronisation with a DP master Problem with start-up synchronization of the PROFIBUS DP master / PROFINET IO controller Profibus DP error End of synchronisation with a DP master In general, what to check: Find the parameters in the connection settings and configure them according to the manual (help in the simatic manager): Finished message from modules (100 ms) Transfer of parameters to modules (100 ms) |
Best Regards |
|
Follow us on