12/27/2012 6:39 AM | |
Posts: 461 Rating:
|
hi Shustrix, Have u tried communicating with any other 214 plc if it communicates then no probelm with ur pc or ppi cable properties. May be as Marcjan said it may be a damaged plc. if not What is ur ppi cable status... I think a led must glow that implies that ur PPI cable is active if not try downloading driver from the below link & try installing it.... https://support.automation.siemens.com/WW/llisapi.dll/csfetch/19136131/PC_AD_USB_V11.zip?func=cslib.csFetch&nodeid=19133809 or https://support.automation.siemens.com/WW/llisapi.dll/csfetch/21226394/PC_AD_USB_V12.zip?func=cslib.csFetch&nodeid=21226938 Hope it helps Regards, Nelliyan.G |
10/3/2013 7:43 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Did you follow the tips in this thread? The figure in your circle is the E-Stand (hardware release)version off the module. How can you determine the "E-Stand"..... The 2 potmeters (that's what they are) you can read out in your program i.e. to adjust timers. Processing the on-board potentiometers CPU214 Regards, Marcjan |
Last edited by: Marcjan at: 10/3/2013 7:56 PMcorrexted link and typo Last edited by: Marcjan at: 10/3/2013 7:45 PMLast edited by: Marcjan at: 10/3/2013 7:44 PMProblem solved? |
|
11/28/2013 12:28 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, i don't believe it's a too old PLC, have a goldy oldy here working fine with Win 7 and Microwin 4 SP9 6ES7214-1AC01-0XB0 . It must be a setting(or a damaged PLC), but because there is no post since10/3/2013, 5:47 PM, i think the problem is already solved or not that urgent anymore. With problems like this it's best to mention the used software versions and the type of interface cable and PLC. regards, Marcjan |
Last edited by: Marcjan at: 11/28/2013 12:29 PMProblem solved? |
|