12/11/2024 10:35 AM | |
Joined: 4/20/2024 Last visit: 8/1/2025 Posts: 7 Rating:
|
Hello, i have atached two pictures, what do you mean by parameters? are they like the 2040 - Exact stop course 1st axis?, i probably have a backup of this... I have the following files from previous backups... PCA, PCP, RPA0, RPA1, RPA2, RPA3, SEA, TEA1, TEA2, TOA, ZOA0, ZOA1, ZOA2, ZOA3... My concern is that the screen is not showing anything (like the actual GUI of the control with all the options and menus), and the red led of cpu card is on... Attachmentpromecor-siemenscontrol.zip (174 Downloads) |
12/12/2024 1:44 PM | |
Joined: 4/20/2024 Last visit: 8/1/2025 Posts: 7 Rating:
|
It is a 810M ga3, picture atached... |
Follow us on