9/1/2025 2:07 PM | |
Joined: 10/9/2014 Last visit: 9/1/2025 Posts: 1 Rating:
|
I am experiencing the same situation where Proneta only detects my laptop … The weird thing is that AvailableDevices on TIA also doesn't detect any devices, but I can download to the CPU and get online with it, but that's about, no other device can be detected, even when directly connected. Anyhow, I read the responses above, or should I say non-responses … I say, if you know the solution to the issue then directly type it, don't say read the manual! most likely the person with problem has done all she/he can do and now resorts to the forum … moronic replies just to reply is wasting time at best. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/02/2025 11:09:31New subject after splitting |
|
Follow us on