9/24/2017 1:56 PM | |
Posts: 49 Rating:
|
Hi All, I have issue on Load Memory. Can you please advise reg this issue. project backup(OFFLINE) Memory – 2MB only but, live system (CPU) memory - 16 MB(100%). so i cannot download the program. I have attached the screen shots also. please advice . CPU- 417-5H Memory card size -16MB process image input -16000 process image output -6000 Diagnostic buffer - 120 Is there any special memory required for above configuration. i really confused. Should i need to configure new memory card or not Thanks, Plug &Play AttachmentMemory Issue.zip (405 Downloads) |
Last edited by: PlUg & PlAy at: 9/24/2017 2:00:25 PM |
|
9/24/2017 4:05 PM | |||
Posts: 49 Rating:
|
Hi dchartier,
I am ok with your concerns, thanks for the update. i will do compress memory but it should not provide so much sound correct?? we already commissioned the plant. i am confused why the memory difference so much. if i am going to insert new memory card means what are the causes in the running plant. is there any possibility to change the memory card to operation mode? while changing memory card, the redundant CPU will accept different size of memory card?? for synchronization? below steps will work or not while i am insert new memory card
if above points cannot means. how can i do this job.please advice. thanks, PlUg & PlAy |
||
Follow us on