3/14/2018 12:40 PM | |
Joined: 12/27/2016 Last visit: 8/19/2025 Posts: 19 Rating:
|
Hi, I have a similar problem as Zvonko. The client already has S7 1200 (6ES7 214-1AG31-0XB0) and he wants to expand the existing system with RFID module (RF120C) which has already been purchased. The problem is that I can't use the function blocks from SIEMENS Ident package which I need for RFID module because I need at least firmware v4.0 I tried to make a software for firmware v4.0 (6es7214-1ag40-0xb0) and then I tried to change the device to 6ES7 214-1AG31-0XB0, but I couldn't do that because TIA portal offered only firmware v4.1 for replacement. I am using TIA portal v13 SP1. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/15/2018 10:54:00 AMNew subject after splitting |
|
Follow us on