9/19/2008 3:30 AM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
you can try download the older version using OS Update .Then try to download the HMI. AttachmentProt_l_e.pdf (505 Downloads) |
Last edited by: Deeps at: 9/19/2008 3:37 AM |
|
9/22/2008 7:00 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi, that is not posssible with the OP15 because the OP15 is not a Windows based Panel. Bye |
10/1/2008 8:11 PM | |
Posts: 4 Rating:
|
Can anyone tell me where can I found a old version from Protool. Thanks manferreira |
10/2/2008 1:26 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi, your answer is in the following link: /tf/WW/en/Posts/13064 =================================== Following OP15 supports ProTool OP15/A 6AV3515-1EB... Firmware must >2.20 OP15C 6AV3515-1MA2... 6AV3515-1MA3... Firmware must >2.20 In case Panel has 6AV3515-1MA0... then it's an OP15/B and only COMTEXT can be used. Same is Firmwares lower 2.20 on the other Panels. To find out which Firmware is on the Panel just need power on and look, after a few seconds the firmware release will be displayed. ==================================== Bye |
Follow us on