9/2/2025 7:58 AM | |
Joined: 9/2/2025 Last visit: 9/2/2025 Posts: 3 Rating:
|
AC MCB has labels of the terminals as LOAD and LINE terminals whereas the DC MCB will have positive (+) or negative (-) sign on its terminal. If the properties of the AC MCB and DC MCB are looked for the differences among them than the only noticeable difference is the breaking of AC MCB and DC MCB. It is harder to break a DC MCB as compared to an AC MCB. AC MCB is extinguished with the help of zero crossings but a DC MCB is extinguished with the help of a mechanical interruption or with cooling. DC MCBs open faster as compared to AC MCBs. For more details, you can check out this article: https://electgo.com/resources/mcb-for-ac |