3/12/2021 11:36 AM | |
Joined: 1/28/2021 Last visit: 7/4/2025 Posts: 11 Rating:
|
Hello, Following a power cut on CPU319, it did not start in run. In the diagnostic buffer, the event is: Event 3 of 10: Event ID 16 # 4301 Switching from STOP to START-UP Cause of STOP: STOP by I / O management Getting started information: - Saving the time for time stamping at the last power-up - Monoprocessor mode Start-up in progress / carried out last: - hot start by positioning the switch; last power-up saved Authorized start-ups: - manual hot start allowed - automatic hot start allowed Last command in force or automatic start-up on power-up: - hot start by positioning the switch; last power-up saved Operating status so far: OFF (internal) Requested operating status: START-UP (warm start) Occurring event 12: 08: 47.196 11/03/2021 (Coding: 16 # 4301 FF46 C772 4548 0813 7713) By activating the stop / run switch, the cpu started normally. On the rack there is only the CPU and a Phoenix Contact card for the Interbus network (IBS S7 300 DSC-T). I think the IBS card is involved, because it probably takes longer to start up than the CPU (I have to test this soon). Can you help me find a solution so that the CPU starts up without intervention on the switch? Can the startup of the CPU be delayed, for example?
Attachment20210311_DEP_TUI_MICROCOUPURE.txt (478 Downloads) |
3/12/2021 12:14 PM | |
Joined: 1/28/2021 Last visit: 7/4/2025 Posts: 11 Rating:
|
Ok ,sorry, The diagnostic buffer in english is in attachment. AttachmentDiagnose.txt (497 Downloads) |
3/18/2021 7:48 AM | |
Joined: 1/28/2021 Last visit: 7/4/2025 Posts: 11 Rating:
|
Does anyone have a suggestion regarding this problem? |
Follow us on