1/31/2022 7:14 AM | |
Joined: 11/21/2016 Last visit: 11/20/2022 Posts: 16 Rating:
|
I didn't want to create new topic and I write here what is original interface PG/PC to s7-300. exactly it is 6ES7 315-6TG10-0AB0. Now I have equivalent 6ES7 972-OCB20-0XA0 ( chinese) and I can't download content from PLC , I see what it is model but when I try download programm all stoping I try communication per profibus , in setup PG/PC I have profibus as activ ------------------------------------------------------------------------------------------ |
Last edited by: uniwel at: 01/31/2022 08:38:33Last edited by: Jen_Moderator at: 01/31/2022 13:38:49New subject after splitting |
|
1/31/2022 7:16 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
to which interface of the PLC you are connected? (the PLC have 2 interfaces)! |
1/31/2022 11:25 AM | |
Joined: 11/21/2016 Last visit: 11/20/2022 Posts: 16 Rating:
|
I connected per MPI |
1/31/2022 11:29 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
and which settings configured for this interface in the project? |
Follow us on