3/10/2022 11:01 PM | |
Joined: 4/8/2020 Last visit: 2/19/2025 Posts: 2 Rating:
|
چگونه می توانم برنامه را از سی پی یو سری 300 به کارت حافظه دانلود کنم؟ ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/11/2022 11:37:53New subject after splitting |
|
3/10/2022 11:02 PM | |
Joined: 4/8/2020 Last visit: 2/19/2025 Posts: 2 Rating:
|
How can I download the program from the 300 series CPU to the memory card? |
3/11/2022 12:43 AM | |
Joined: 9/27/2006 Last visit: 9/8/2025 Posts: 12401 Rating:
|
Hello Khancity; Thank for translating uour question from the Arabic, it helps more participants understand what help you need when you are on the Siemens forum. To give you a definitive answer we would need to know the part number of the CPU you are working with, and the memory card you are using. This will help us inderstand how old the CPU is, and the memory card format you have. There have been a few generations of S7-300 controllers, some with ROM or RAM memory cards, the newest models use a micro memory card (MMC). This link will show you the different generations of S7-300 CPUs and how they use memory cards as load memory: https://support.industry.siemens.com/cs/ww/en/view/7302326 In the case of the lastet models of S7-300, simply dowload the program files to the CPU, using Step 7, and the program will be written on the MMC. Hope this helps,. Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on