5/30/2022 7:02 AM | |
Joined: 5/30/2022 Last visit: 5/30/2022 Posts: 1 Rating:
|
Hello, can I use a newer model like 318-3FL01 cpu instead of 318-2DP cpu? ------------------------------------------------------------------------------------------ Attachment6ES73183FL010AB0_datasheet_en.pdf4_.pdf (834 Downloads) |
Last edited by: Jen_Moderator at: 05/30/2022 12:15:16New subject after splitting |
|
6/13/2022 5:57 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Your Old CPU is 318-2DP. Your new suggested CPU is 318-3F "Fail Safe Type". So it seems that you will use fail safe CPU in standard mode. If this is the case, you won't need any addon package. TAnd as friends told you here that CPU 318 is a very special CPU with 4 ACCU. So, to choose an optimum successor, you have to use the CPU 318 Migration Check tool. You will upload the software to it and it will check for you to tell if the optimum successor is CPU 317 or 319. for more info, please read the following FAQ: |
Ayman Elotaify |
|
Follow us on