1/13/2010 1:36 PM | |
Joined: 9/28/2005 Last visit: 7/24/2025 Posts: 2957 Rating:
|
Hello, If your HW configuration and wiring is ok then you read current the same way as voltage. I normally use Load command: [code]L PIWxxx[/code] And scaling is simple. If your input is configured as 4..20mA then you read value 0..27648 respectively. Look at this manual chapter 5 to have bigger knowledge about how analog values are represented in S7-300 PLC. |
Best regards, |
|
1/25/2010 2:00 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Dear bite me, Please have a look on these links. It's usefull. How 27648 Analaog Maximum Value ? How and for which analog measurements can you use the function FC105 "SCALE" to convert the integer values (INT) into real number values? Regards, |
Ayman Elotaify |
|
Follow us on