5/10/2008 9:22 AM | |
Posts: 69 Rating:
|
Dear Sir, i having a Laptop installed with Step 7 V5.3. i am facing a problem with a project whose hardware consist of CP341 in ET200M Station. Problem: When i want to insert the CP341 in spare slots in Hardware configuration, i am not able to do it. i am receiving error as attached with this mail i.e. "Unable to create object"(error_2.bmp as attached). also, note that if i am making s7 project with CP341 in differentComputer and then i try to open in my laptop, i find different error(error_1.bmp as attached)while opening the project in SIMATIC Manager. what may be the problem with my laptop? Please, help.
AttachmentCopy of errors.zip (356 Downloads) |
5/10/2008 12:59 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi John, I think that you have to install the option package for the Serial Cards, you can download that under the next URL : Download CD "CP340, CP341, CP440, CP441" When you use a special driver, for instance Modbus or DH from AB then you may download those drivers also. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on