9/3/2008 4:35 AM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
Hi Jane The Manual for 13 AI Module you can find out on following link.Check Chapter 6.6 for 13 bit AI https://support.automation.siemens.com/WW/llisapi.dll/8859629?func=ll&objId=8859629&objAction=csView&nodeid0=10805045&ehbid=html%5F76%2Fehb%2F8859629%2Ehtm&nodeid=10072094&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=content&csQuery0=AI Module &subtype=133300 As far as SF on AO Card you can check the following basic things 1.Check the hardware configuration of AO card in step 7 & Physical Card should match. For Example the if chanel is set for current/ Voltage accordingly the Jumper at back side of card is required to set. 2. Check the wiring of Analogue outputs for correctness . I hope this will help you to resolve your issue. |
Last edited by: Deeps at: 9/3/2008 4:36 AM |
|
9/3/2008 8:08 AM | |
Posts: 17 Rating:
|
Remember, check Hardware Config in the project. See also HELP here. |
9/3/2008 8:52 PM | |
Posts: 2 Rating:
|
Thank you all for answers, helped me a lot!!! |
Follow us on