12/17/2008 8:05 AM | |
Posts: 433 Rating:
|
Hi BazzLightYear, another possibility to FB125 is the "Systemdiagnostics". But without parameters there is no way. Tomcat |
12/17/2008 8:31 AM | |
Joined: 5/25/2007 Last visit: 9/1/2025 Posts: 83 Rating:
|
Dear Tomcat: Thanks for your reply.I'll tell my customer about the usage of the solution best regards Buzz Light Year |
12/17/2008 10:25 AM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Dear BazzLightYear, The FB 125 is for visualization for faults in a Profibus networks. Sure you can see if there's a wire break or not using this way. If you just need the information, you can use RSE (Report System Error). You will know what's wrong through messages. You can easily configure what kind of information you exactly need in these messages in SIMATIC MANAGER. If you are interested, take a look at RSE for WinCC RSE for WinCC Flexible Another way you can use to detect the wire break is to make a quick function with little comparison todetect the wire break. I've attached a PDF file where you can see how the analog value is represented in S7 CPUs. Best regards. AttachmentAnalog value representation.pdf (664 Downloads) |
This contribution was helpful to
2 thankful Users |
12/18/2008 10:14 AM | |
Joined: 5/25/2007 Last visit: 9/1/2025 Posts: 83 Rating:
|
Dear H-H: thank you,I'll test the RSE function in winccv62. Best regards Buzz Light Year |
Follow us on