3/21/2022 9:14 AM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating:
|
Any Help Please !! |
3/21/2022 12:12 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12401 Rating:
|
Hello Escanoor; The forum has some communication issues these days, personnal messages do not get through, and some replies do not appear when we post them. Please be patient. A CPU 314C-2DP is designed for programming over a Profibus-DP interface, and the CP 5711 is a standard tool that normally works very well. Until recently, you said that you were using it without any issues. So, either thr CP 5711 now has developed problems, or the connection to the PC, or the DP port on the PLC. Start with the CP 5711: what are the status of the operation LEDs when you try to connect it to the CPU? Look here at the CP 5711 manual for more details: https://support.industry.siemens.com/cs/ww/en/view/34803449 Hope this helps, |
Last edited by: dchartier at: 03/21/2022 14:58:22 |
|
3/21/2022 12:41 PM | |
Joined: 3/30/2020 Last visit: 9/9/2025 Posts: 5434 Rating:
|
This forum is mostly driven by unpaid volunteers. Consider speaking to Siemens directly by registering for free support: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
3/21/2022 1:14 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating:
|
hello Mr Daniel
But when i disconnected the cp5711 and use the PC adapter it still the same probleme !! |
3/21/2022 1:28 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, have you tried via MPI port (on the left)? |
3/21/2022 1:36 PM | |
Joined: 11/24/2021 Last visit: 7/21/2023 Posts: 37 Rating:
|
yes , i tried and same probleme . |
Follow us on