4/10/2021 8:20 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, technically, this looks to be possible. Ideally, for minimum fuss, You either need to download the firmware version (assuming it is still available for download) or transpose it from the old card onto the new. If You did manage to download the EXACT same version of firmware and unzip it onto the card, then simply overwriting the USER directory on the new card with that from the old card should be enough to end up with an operational system. If You can't download the old version and the old card is corrupted, then You would have no choice but to upgrade the firmware version to the latest version downloadable for a D445 which is available HERE The firmware support packages for Simotion Scout in the event You need to upgrade are downloadable from HERE Regards, Graeme |
Last edited by: Jen_Moderator at: 04/12/2021 08:56:12Optimized links. |
|
Follow us on