(1)| 3/3/2020 11:38 AM | |
|
Posts: 1 Rating:
|
Hi, I downloaded and burned into a SD the latest v2.6 from LINK. No mods. Started the IOT2000 with no problems, set a static IP via iot2000setup, turned on the Autostart of Node-red, and no other config is touched. System rebooted, and when I type in my browser: http://<IP ADDRESS>:1880 nothing happens. Tryed to start via:
and this is drop:
So maybe the node-js install is broken in the new release v2.6? I burn the card with Win32DiskImager without any mods, and I have tryed two diferent SD cards. Any help is appreciated. Best reggards. |
Last edited by: Jen_Moderator at: 03/03/2020 13:25:10Optimized link. |
|
| 3/3/2020 11:47 AM | |
|
Joined: 4/28/2015 Last visit: 1/7/2026 Posts: 578 Rating:
|
It's installed under /usr/lib/node/node-red/ now. You can also auto-start it via iot2000setup. |
| 6/10/2020 7:03 PM | |
|
Joined: 6/8/2020 Last visit: 11/1/2023 Posts: 1 Rating:
|
I have the same problem!! could you solve it? |
| 4/20/2021 10:45 PM | |
|
Joined: 9/27/2006 Last visit: 8/21/2025 Posts: 47 Rating:
|
Thanks! I has having the same issue and it is working fine now. I was following an outdated manual:S7 communication with node-red |
Follow us on