(1)| 5/17/2021 11:27 AM | |
|
Joined: 10/11/2006 Last visit: 1/7/2026 Posts: 6 Rating:
|
Hello, please refer to the compendium and the function diagrams. U530 is the connector input for the controls signals for positioning (see function diagram 809) and U531 to U533 are the connector inputs for G function, position and speed in MDI mode (see function diagram 823). |
This contribution was helpful to
|
|
Follow us on