5/29/2021 11:43 AM | |
Joined: 9/21/2012 Last visit: 9/17/2025 Posts: 4714 Rating:
|
If you can't connect to the CPU, then you can't do a wipeout either... |
5/30/2021 4:51 PM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
so the PLC is Faulty? |
5/30/2021 11:28 PM | |
Joined: 3/9/2018 Last visit: 9/3/2025 Posts: 208 Rating:
|
If you power up the plc in stop mode the SF LED is on? |
5/31/2021 9:51 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
yes |
5/31/2021 9:54 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
I Tried wipeout but I can't use it on windows 7 64bits it need 32bits, there is one which work with 62 bits? |
Follow us on