10/5/2021 2:25 PM | |
Joined: 4/28/2015 Last visit: 4/17/2025 Posts: 9 Rating:
|
Hello jameskkk, there is an example project including the manual (05/2021) in SIOS. In chapter 3 and 4 you will find an explanation how all the blocks are used in combination. The example is also described in the manual and you can open it in your TIA. Additionally feel free to apply to the application support (see chapter 6.2). of the manual You can write to that address and explain your application and ask for support. With best regards, |
This contribution was helpful to
1 thankful Users |
10/5/2021 4:38 PM | |
Joined: 5/18/2018 Last visit: 7/5/2022 Posts: 4 Rating:
|
Hello Stephan: Thanks for your help! For the question I raised maybe is not described clearly, now I want to give out again. The project has three Axis, one is leading axis(LineFB), one is Winder(LineFB), the rest is Traverser, now I applied ProjectGenerator to configure a Module converting, so I got a Project with Leading axis and Winder axis by this way, the project also containing the program to control two axises. The Traverser axis need following axis according to the specification, but the ProjectGenerator can not configurate the following axis(LineFB). so I dont know how to integrate the Traverser to the project and be controlled. I read some help from converting manual, the attachment shows a example like my project, but I don't know where to get it, please find the attached manual in page 30. Could you please help me to find out this example? waiting for your reply. best regards! James.Liu AttachmentManual_TraversingDrive.pdf (858 Downloads) |
Follow us on