12/23/2021 8:49 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 5444 Rating:
|
Hello. The question is very generic. I am having a difficult time to decide what exactly you want as an answer. There is a document that has been very helpful to me; the current version is: I will use REL and ABS as shorthand in some quick introductory notes.. REL and ABS starts a task if triggered with a boolean trigger that transition from FALSE to TRUE. It will continue the task until finished or a process interrupts / override it. (see manual) Note that the target speed cannot change while the REL/ABS block is doing a movement. REL is for moving a distance. The starting position is not of importance. Only the current position is of importance. A negative distance is always in the reverse direction. ABS is movement to an absolute position. The reference position is set by using the MC_HOME instruction. No movement is allowed if the reference / homing position is not set. The reference is also lost when the enable (MC_POWER) is lost. +/- on the position request does not indicate the direction. The target position is always measured against the reference position. For your stepper motor.. What of these notes did you already know? ~ |
Last edited by: qwazee at: 12/23/2021 08:53:10add notes for stepper motor Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on