2/9/2022 5:25 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please refer below examples. may help you. SIMATIC S7-1200 / S7-1500: Encoderless Positioning with SINAMICS G SINAMICS G: Axis positioning with the "SINA_POS" block SINAMICS S/G/V: Simple cyclic Funktions Blocks for Controlling a SINAMICS in TIA Portal |
Last edited by: Jen_Moderator at: 02/09/2022 09:24:27Optimized links. |
|
2/10/2022 6:20 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Yes. |
This contribution was helpful to
1 thankful Users |
2/10/2022 10:14 AM | |
Joined: 8/21/2018 Last visit: 9/11/2025 Posts: 96 Rating:
|
Hi daviso, you are right, my question is not precise. So I will try to ask more clearly. I am looking for possibilities to positioning of G120C drive (not G120 but G120C). I know how to use EPOS with G120, but I never heard about something like that to G120C system. But when I added G120C to my project and tried to configure Positioning Axis I could choose option "Analog drive connection". Then I can specify the analog output which will control the drive. The encoder I can connect to HSC interface. I attach the screens with that configuration. I have never heard about such a configuration before, so I have doubt if it will work correctly ? Also I can choose drive option as "PROFIdrive" and then choose telegram in drive Tab (see on Screen 5) but DP_TEL1_Standard sound strange for me. So did You ever try to control G120C in this way ? Will it work ? Thanks for yours answers, Best regards, Rafał
AttachmentNew folder.zip (410 Downloads) |
Follow us on