2/15/2022 9:10 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
You can use a TO_ExternalEncoder and then perform homing. |
This contribution was helpful to
1 thankful Users |
2/16/2022 4:16 PM | |
Joined: 11/4/2011 Last visit: 9/10/2025 Posts: 276 Rating:
|
No, you cannot. According to the originator of this thread, this is about using the 1PosU module, which is not compatible wiht the S7-1200/1500 motion TOs (at least not straight ahead; of course with TO to DB connection and manipulating in OB MC-PreServo/PostServo you could connect anything to the TO...). Regarding resetting the encoder value of the 1PosU: One way might be using this function of the module, perhaps: https://support.industry.siemens.com/cs/de/en/view/45977481/540367755 Regards, |
Follow us on