(1)| 4/12/2009 4:20 PM | |
|
Joined: 5/28/2008 Last visit: 1/12/2026 Posts: 4522 Rating:
|
Arindam Chaudhuri wrote in a privite message:
Hello, No. There's no need for interfacing devices as Siwarex modules in general is designed to read the weighing signals directlly from the load cells. More over there's an integrated I/Os on the FTC module and you can use it and you have to program it. Here's under a links for the manuals of Siwarex FTC modules and I think it would be useful for you. http://support.automation.siemens.com/WW/view/en/26043227 http://support.automation.siemens.com/WW/view/en/29501218 Regards, Ayman Elotaiy |
Last edited by: Ayman Elotaify at: 4/12/2009 4:22 PMLast edited by: Ayman Elotaify at: 4/12/2009 4:20 PMAyman Elotaify |
|
| 4/14/2009 9:14 AM | |
|
Joined: 1/4/2007 Last visit: 1/13/2026 Posts: 1198 Rating:
|
Hello Ayman Elotaiy and Arindam Chaudhuri, Attached you can find a circuit diagram, how to connect the MD256 to a Siwarex FTC module. Please note: With a new MD256, you can also use a 24VDC power supply instead a 15VDC power supply. Best regards Siwarexi AttachmentMiltronics_Speedsensors_with_FTC.PDF (492 Downloads) |
This contribution was helpful to
|
|
Follow us on